Other Parts Discussed in Thread: LM3495
Hello
I made a set up with the LM3495 EVALUATION BORAD
i took a new evaluation board and try to limit the current at 1A so i use as Rilim=500mOHM, that work perfectly
-Now i want to have an output votage of 3.7V with 12V as a Vin,
i changed the Rfb2 = 51.3kOhm with the current limitation at 1A with a load of 2 Ohm, i don't have the limitation at 1A i got 2.24A
I don't understand how the Rfb2 modification can impact the current limitation.
best regards,
Adjagbe