Hi team,
When EN=0, and I pull up PG to VCC, how about the statue of this pin? Will it be in low state or follow the VCC signal? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
When EN=0, and I pull up PG to VCC, how about the statue of this pin? Will it be in low state or follow the VCC signal? Thanks.
Hi ,
PG is the open drain output of a voltage detector. The output voltage must be pulled up to a voltage in order to generate a logic high signal when the internal pulldown FET is OFF; however, this voltage used as the pullup will not impact the function of the voltage detector. When Vout is less than Vit(pg) + Vhys(pg), the PG output will be logic low. As such, when the regulator is disabled, PG will be logic low.
Very Respectfully,
Ryan