This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895: Reliability with 14.4V Input

Part Number: BQ25895
Other Parts Discussed in Thread: TPS2595,

Hi Team,

My customer is looking at using the BQ25895 with a solar panel input that will be typically 12V/1.25A. However, the input can go up to as high as 14.4V/0.2A for a duration of about 2s every 10 minutes or so worst-case. The max recommended for the device is 14V. However, given that the abs max is 22V, would you expect any long-term reliability issues with this application? The alternative would be to add a clamping eFuse such as TPS2595 but they wouldn't want to do it unless there's no other option.

Thanks,

Antonio