Tool/software: WEBENCH® Design Tools
I am currently trying to find a low voltage, low current Buck converter that could meet these requirements:
Vin = 6-17 V, 12V nominal with an Output Voltage of 3.3V @ 3A with a max deviation of 3% for all line, load and temp variations.
Temp ambient : -40 C – +85C.
Within a 645.16mm^2 footprint.
The customer requires the highest efficiency possible.
Please let me know if there are any specific TI parts that could fit these requirements other than the TPS565208.
Thank you