As 3.3V systems get more common I am interested in LM4041A12ILP to test the reference and the design on breadboard. Is there any information when will it be available in TI WebShop?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Laszlo
I will check with marketing team and let you know.
However LM4041C12ILPR is available on TI web store.You can use this part if you are okay with 0.5% initial accuracy (All other parameters are same as A grade).
Regards
Trailokya
Hi Trailokya,
I am working on DVM and 0.1% (or even better ) means 3 digit without calibration, so I prefer this product.
Thank you for your kind help!
Regards,
Laszlo
Hi Laszlo,
We currently do not have plans to release this device in TO-92. If you just need this device in a package to test on a breadboard for prototype, I personally use the EVM dip adapter boards to use these devices on a breadboards.
Hi Laszlo
It will be good if you try other shunt references with 0.1% accuracy as suggested in previous post because they are easily available.
However the exact replacement to the LM4041A12ILP is the LM4041AIZ-1.2/NOPB.
They both have the same exact specs in accuracy 0.1% at T= 25C, and for T=-40 to 85C, they are both +/-9.2mV.
Additionally, the ppm/C is exactly the same at 15 ppm/C typical and 100ppm/C max. You can try this for TO-92 package.
Regards
Trailokya
Hi guys,
I think adapter board not the correct solution, I could solder lead for the SOT package and I can test, it but it looks terrible. Additionally, If I need higher precision I can use LM5050 but that has no 1.2V version.
So, I think it has no good solution right now and I hope there will be enough interest for this reference to change your mind.
Regards,
Laszlo
Hi Laszlo,
The LM40xx families are divided into 2 parts.
The LM4040 and LM4050 are the 2V and higher fixed references.
The LM4041 and LM4051 are the 1.2V and adjustable versions.
Please check out the LM4051-N for a 1.2V reference
If you need a lower Iq 1.2V with high precision you can look into the REF1112.
-Marcoo
Hi Marcoo,
it is a nice collection of voltage references but everything is in SOT-23. Advanced users can solder SOT-23 and I plan to build for sale with surface mount version.
Right now, I am designing DVM for beginners as a kit and they cannot work with small SMDs. TO-92 package version at least from a selection of voltage references would be important.
I know it is not a big market but maybe if you produced LM4041A12ILP for a dedicated order, would make sense to produce additional 1000 pcs for TI Webshop.
Regards,
Laszlo