This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61165: Can't control LED brightness by PWM.

Part Number: TPS61165

Hi,

I trying to control de two LEDs brightness by PWM (5kHz and 10kHz), however, for any duty cycle I have used, the brightness remains the same. 

Any suggestions appreciated

       Component list:

  • D1: MBR0540T1G
  • C1: 4.7µF, 10V, X5R CL10A475KP8NNNC
  • C2: 220nF ±20% 6.3V GRM033R60J224ME15D
  • C3: 1µF, 10V, X7R CL10B105KP8NNNC‎
  • R3: R1 0.3Ω, 0.5W, 1% RL1632R-R300-F
  • L1: 10µH, 1.49A  #A915AY-100M=P3  murata
  • LED:  LXML-PB01-0030