Part Number: LMG3410R070
Can you please elaborate the third quadrant operation of LMG3410R070 and provide the Vsd vs Isd curve variation with Vin.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMG3410R070
Can you please elaborate the third quadrant operation of LMG3410R070 and provide the Vsd vs Isd curve variation with Vin.
Hello Kousik,
Thanks for your interest. The explanation on third quadrant operation is given in Section 8.1 in the datasheet of LMG3410R070. The Vsd vs Isd curve is also provided in Figure 4 of the datasheet. I'm not very clear on what you mean by Vin. Could you explain it further?
Thanks,
Serkan
By Vin I mean the logic pulse input to the IN pin. Which is to be varied between 0 & 5 V. Figure 4 shows the curve for IN =0V . I want to know the curve for IN=5V. Section 8.1 describes the 3rd quadrant operation, when GaN is turned OFF. I want to know the source- drain voltage drop when GaN is ON.
Hello Kousik,
When IN=5V, the device turns on and shows a resistive behavior in the linear region of operation. You can see the waveform in Figure 3. The gray line in that figure shows the OCP limit. Once the device current goes above this limit, OCP block will cease operation.
The RDSon will have a temperature dependence and increases as the junction temperature goes up. This behavior is also shown in Figure 5.
Please let us know if you need more information.
Regards,
Serkan
Figure 3 shows the first quadrant characteristics. I want to know the third quadrant characteristics when IN=5V. (Figure 4. shows the third quadrant characteristics at IN=0V). Can you please elaborate this ?
Behavior of GaN when Vin=5V when current is negative, is same as 1st quadrant operation. There is no offset voltage drop, but just Rdson. You can check this from Figure 4 of SNOAA36 app note.
Thanks,
Serkan
Well, but the pspice model of LMG3410R070 released by you does not agree with the characteristics shown in Figure 4. of SNOAA36. In the above mentioned model, there is a continuous offset voltage drop of 7.5 V when operated in third quadrant. Also there is no dependency on Vin when operated in third quadrant (pspice model). Please see to the matter and let me know, whats the problem in the pspice model.
Hello Kousik,
I thought you were referring to 3rd quadrant when IN=0V. There shouldn't be any offset issue when IN=5V. I'm investigating the issue with the pspice model. I will get back to you with an answer soon.
Regards,
Serkan
Hi Kousik,
New model has been released on July 12th. Please download the newer version. There shouldn't be any offset issue when IN=5V. If you still experience problems, please let us know.
Regards,
Serkan
Thanks. I checked the revised PSPICE model and its working fine. The vsd voltage drop irrespective of IN voltage is removed. It is operating as expected in third quadrant.