Designed a 3Kw PFC with half bridge following.
1] The values shown in the Excel design tool spread sheet are confusing at best. Example it shows RTA and RTB to have values of "-1.41e+03" How can there be a minus sign?
2] The values f many parts are way different from typical TI schematics.
3] For our design the current sensing XFR [Line 39] is shown with a turns ratio of 1:491. There is no information regarding what turns ratio should be used for a particualr power output design.
4] Some designs show a diode + 33v zener acrosso the current sense secondary, others show a snubber (4.7pF + 1K) yet the spreadsheet calls for 100R for 3Kw...confusing so which is correct? Snubber or diode snubber?
5] In line 84 the value called for is 5.9E-10 but in line 85 the value shown is 2.53E-09
Hope someone can clarify these issues
Steve