This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65950/30/20: Customer questions and clarifications (Rrtso, DP, DM)



Following are questions from customer:

1. For 7.2.4.1, 5-V Tolerence, could we understand that when voltage on DP/DM > 3.6V, the output of VRUSB_3V will be charged as high as 3.6V? If yes, is there a range for this value? We couldn't find it from the table.
Also, for table7-6, the unit is h for "continuous short-circuit stress". Is h "hour"? Does it mean that we have tested at least 24hours w/o problem?

Yes, it is hours. VRUSB is a range. It will charge upto 3.6V depending on voltage on DP/DM


2. For table 15-1, Rrtso is 22ohm/100ohm. Does this mean Rrtso is 22ohm or 100ohm? Or from 22ohm to 100ohm?

Rrtso resistor value is a range and the customer can have any value in this range to adapt to his board/hardware.