I am using UCC27511 single channel gate driver to drive 700W LED module (Output Voltage 375 to 390). We are implementing non inverting driver configuration as in application note (Fig 25 in datasheet) to drive mosfet PSM20N60CT. I am using R1 = 5.1ohm and R2= 0.5ohm as gate resistors and a gate to sourse resistor of 10K. The problem i am facing is that the gate driver and mosfet is getting failed if i connect the load for around more than 1 hour.
But the same LED module is working if i use the UCC28180D gate driver.
Please help me.