Other Parts Discussed in Thread: TPS62840, TPS62808
Hi,
I would like to use the TPS62748 to regulate a 3.7V lithium polymer battery to 3V. The system could consume up to 350mA but will be mostly in low power mode (10µA). In the datasheet it seems that below Vout+0.7V the current is limited but it does not state what current can be achieved with lower headroom. What current can I expect at 3.2V input for 3V output?