This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The power line to meet the load dump for automotive

Other Parts Discussed in Thread: LM5146-Q1, LM5085-Q1

Hi


I search the devices or reference design to be able to meet the following spec.
Are there the reference design to meet them?

 Vin:8~110V(Vin_max=141V at load dump)
 Vout:3.3V
 Iout:5A
 Rating:Automotive

Best regards,
Yokota