Other Parts Discussed in Thread: LMG1020
Dear,
I am using this module to drive an infrared LED (OSRAM SPL PL90).
Before attaching the LED to the module I tested the module without removing the resistors, just as it came out of the box. I measured IN+ and Vg and I got a proper signal, at 100KHz and 100ns pulse width as recommended in the manual. Then I measured the voltage at Vbus (TP5) and I can see a signal following the Vg, this in principle should tell me that the FET is switching properly, but I can see that this Vbus voltage has an offset of -1.92V. I am a bit puzzeld about it and it is very important for me to fully understand the issue. I am afraid that if I connect the LED I will damage it becuase of exceeding absolute ratings when reverse biasing the LED because of the offset.
I will really appreciate your help and guidance.
Regards,
Juan