Hello TI
I want to use two or more chargers in parallel application, but i expect to use one total power sharing.
Can I connect the current sense resistor in series to achieve this function? Is there anything that needs attention?
Please refer block diagram as below, series RAC1 and RAC2 share the same total power.
If the above is feasible, how should the ACDRV & CMSRC pin be connected?
Can I let it float or connect together?
Thanks a lot
Matt