Other Parts Discussed in Thread: TPS1HA08-Q1,
Hello Everybody,
I noticed by comparing pins / pin-function of TPS1HB08-Q1 and TPS1HA08-Q1 that if I like to set analog current limit I can't use FLT / ST flag anymore (Pin 5).
Was it necessary to use same Pin if you have two of NC (Pin 12 + 13) on both parts?
Then so I can’t use FLT - flag (to disable µC and/or power stage immediately) and set current limit.
The background of my question is this: both functions are great for functional safety purposses! With follow additional benefits:
• Provide fault indication when DIA_EN = 0
• Provide fault indication regardless of SELx pin conditions
• Provide fault indication to a simple digital I/O (rather than ADC or comparator used with the SNS signal)
Why chose between?
Thanks in advance