i need the spec for undervoltage protection in bq77915, values to be used. and if possible an external cell balancing circuit diagram linked with bq77915
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
i need the spec for undervoltage protection in bq77915, values to be used. and if possible an external cell balancing circuit diagram linked with bq77915
Hi Jishnu,
The datasheet shows the undervoltage accuracy in the Electrical Characteristics tables. It is +/-18mV at 25C, and the spec is a little wider over different temperature ranges (see page 7 of the datasheet).
This video about BQ77915 Cell Balancing has an example schematic with external FETs: https://www.youtube.com/watch?v=wewL0oJRBNM
External FETs are needed only if the balancing current needs to be higher than 50 mA.
Best regards,
Matt