This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5024: LP50X: Pin output at exactly 0% or 100% PWM

Part Number: LP5024
Other Parts Discussed in Thread: LP5036

I would like to know if the device has a glitch free output for pins being driven at exactly 0% or 100% PWM.
In other words, if I configure a given channel to 100% brightness and 100% color, will that channel be a steady active open drain digital output?
And if the channel is set to 0% brightness and 0% color, will it be constantly tri-stated?

Usage case: employ "left-over" output pins of the device as common digital outputs to drive other CMOS logic.

I am guessing the same answer will apply to LP5032, LP5036, correct?