Other Parts Discussed in Thread: CSD25402Q3A,
Output of the ic is not as per expectations. According to calculations it should be 4.2V but I'm getting output around 5.3V.
Output voltage waveform nature in no load condition is as per expectations but during load condition it's entering into soft start.
Voltage at feedback pin is around 1.5 V whereas it should be between 0.8 V and 0.82 V.
Components used:
MOSFET used is CSD25402Q3A
Diode used is SD1206S040S2R0
Rfb1 = 47k ohm
Rfb2 = 11k ohm
input capacitor = 470 uF (electrolytic) + 47uF (ceramic)
Output capacitor = 220 uF (aluminium electrolytic) + 47 uF (ceramic)
I'm attaching snaps of output waveform below.