This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22968-Q1: Questions on specifications

Part Number: TPS22968-Q1
Other Parts Discussed in Thread: TPS25940-Q1

Hi,

    Does this chip have protection function?

     There seems to be no explanation in the specifications.

thanks.

  • Hi Wu, 

    Thanks for reaching out on E2E!

    What protection features are you looking for, specifically? The TPS22968-Q1 has controlled slew rate and QOD. However, if you're looking for current limit or overvoltage protection, then the TPS22968-Q1 does not have these features. 

    If these protection features are required, would a device such as the TPS25940-Q1 work here?

    Thanks,

    Arthur Huang