Other Parts Discussed in Thread: CSD19537Q3
Hello,
I am trying to implement a CC Buck and am using this application note as my guideline http://www.ti.com/lit/an/snva829/snva829.pdf. My input is 57 volts and I want the output to give constant 6 A over a 20-45V range at 300 kHz. I used the provided excel file to size my components and the complete circuit is given below. The switches are CSD19537Q3 http://www.ti.com/product/CSD19537Q3 and the inductor is Coilcraft XAL1510-333MEB https://www.coilcraft.com/xal1510.cfm
I am using an electronic load in CR mode as my load right now. When the load resistance is >14 Ohms the converter gives a stable CV, but the switch node looks odd (see attached). When the load resistance drops below 14 Ohms the converter becomes unstable, presumably because it begins to enter CC mode and something is wrong. Any insight into what I could be doing wrong would appreciated and I can provide additional probe images if needed.
Thanks
1033.lm(2)5117_quick_start_hv_calculator V1.5.xls