Part Number: TPS62110-HT
Hi There
The functional block diagram (page 9) and description (page 14) on the datasheet describe a comparitor and an open drain output on the LBO pin. I'm unsure if the comparitor is internally connected to other parts of the TPS62110-HT and shuts the device down?
If a LBI event doesn't shut the TPS62110-HT down then i would like to use this to trigger a uP reset elsewhere in the circuit via the LBO, could you confirm if this is possible or not?
Kind Regards
Martin