This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25120A: bq25120A power up problem

Part Number: BQ25120A


Hi Team,

Can you help to solve some problem with bq25120A.

I encountered problem during power up.

The problem is :

  1. When fully charged battery connected without charger I unable to configure charger to other voltage different from the default.
  2. Same code when battery and after connected charger everything works properly.
  3. When only charger connected also everything works properly.

It’s mean when the battery connected I unable to communicated with charger .

This issue is very urgent, can you clarify?

Thanks,

Shlomi