This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2373-4EVM-758: Duty cycle cannot be adjusted

Part Number: TPS2373-4EVM-758
Other Parts Discussed in Thread: PMP21318, TL431, UCC2897A

Hi ,

My design is exactly the same as 8228.PMP21318_RevA(001)_Sch.

On my circuit board, I found that the duty cycle is not adjustable, and the duty cycle is always the maximum output.Working normally at 12V 5A( 90% efficiency), and the ripple is normal 50mv.Among them, the circuit near TL431 has great interference, resulting in the lifting of load, TL431 K level is always 11v, almost unchanged, resulting in the optocoupler feedback voltage at the other end is always 3.3v (TP23), thus the duty ratio is the largest, always the same.What may be the cause of this problem?I am now testing the external power supply.

My schematic

原理图.pdf

Reference schematic

7411.8228.PMP21318_RevA(001)_Sch.PDF

The 12 v OUT ripple

TL431 K ripple