Hi
Ive been running into some issues getting my IC handle the different kind of load on the secondary side of the transformer, its hard to say if its been the controller loop or the compensation voltage that makes the IC burn out during start up or if its the overshoot on SWITCH-pin.
Im running at a voltage of Vin=29V and clamped earlier with a TVS of 27,6V in serie with a SMA diode but, lately i've tried with a 15V zener diode instead of TVS.
With zener ive increased margin with 12V so now im not near the 65V stand-off, that switch-pin can handle.
The design is build up using the application report http://www.tij.co.jp/jp/lit/an/snva005b/snva005b.pdf
I use all windings in the transformer WE-FLEX EFD20 and has 3 types of voltage outputs, one 5V isolated whitch I take down to 3,3V afterwards with a separate 0V groundplane and also one 5V none isolated with the same 0V groundplane as the 29V on the primary side.
Is it possible to be contacted by email to sort this out?