Hello,
I am planning to use TPS24741 for my application and I have a couple of questions:
1- The input to my circuit (which this IC is part of it) is 12V DC. I have two lines inputs: 1- onboard power 2- Shore power. Both powers are provided by 3s batteries so their voltage may drop lower than 10V. I would like my circuit to connect to shore power even if its voltage is lower than onboard battery. In other word, if shore power is presented, always connect to shore power regardless of its voltage. Is it possible to do this with this IC?
2- My system is rated for about 7amps (at 12V) continues current and about 25amps max current. Is this IC capable of handling that power?
3- I am planning to use the recommended values given in Figure 45 and the schematic given in Figure 60. Is it a good idea or I need to recalculate them for my design?
4- The AUX schematic of Figure 60 is given in Figure 61, but not the main circuit! Shall I use the same schematic given in Figure 45 for Main supply?
5- In Figure 60, it is not clear to me what is Hotswap boxes? Are they inside TPS24741 chip or they are a different circuit?
Thanks,
Babak