This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65400: Turn on the power supply without I2C configuration

Part Number: TPS65400

Hi,
I have a problem with my PCB design. Unfortunately I make a design without considering the I2C access for the configuration.

I would like to ask you, if:

  1. There is a quick way to set un the IC without program it? I measured the generated voltage VDDG, VDDA and VDDD and ar all ok. the problem is that the value of the 4 EN channels are set to '0'. I can connect it for example to VDDD or VDDG or VDDA?

  2. If the only solution is to configure it via I2C. Could you help me providing advice in how to set up the IC. I need a basic way to turn on the 4 channel when I plug the VIN. Without order sequence or other issue.

Thank you for your big help
Best regards

Andrea