This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
We plan to use TPS61088 for 5V/3A 9V/3A 12V/2A application, and external R/C value will try to follow it's EVM TPS61088EVM-677.
As for Cout, we plan to use [ceromic cap 22uF/16V*1pcs] + [Conductive Polymer cap 47uF/16V*2pcs], is it OK?
Thanks,
Hugo
Hi Hugo,
What is the ESR of the 47uF Polymer cap? Could you please post its datasheet?
Hi Helen,
Please refer to attachment.
ESR max@100kHz -> 45mohm.
PN : TCJX476M016R0045
Thanks,
HugoTCJ DTSH 07_18.pdf