This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28C42: Slope Compensation for a Buck Converter

Part Number: UCC28C42
Other Parts Discussed in Thread: INA181

Hello,

Would the slope compensation circuit shown in Figure 27 of the UCC28C42 datasheet also work for a buck converter topology?

Thank you, Keith

  • Hello Keith,

    You can use that circuit with a forward converter which is just another name for a transformer coupled buck converter.

    The difficulty with the buck converter is that the switch current is not referenced to ground.

    As in the drawing below:

    So the figure you attached is not suitable for this type of buck circuit.

    Regards

    John

  • Thanks John.

    Are you saying we could add in current shunt like the INA181 to reference current on the high-side?

    Or is it not possible to do buck converter slope compensation?

  • Hello Keith,

    Your question was whether the circuit your referenced was suitable for a buck converter.

    My answer was that you will not see this circuit in a buck.

    But youu will need slope compensation for current mode control whenever the duty cycle is greater than 50%

    As far as I know the INA181 has a very low bandwidth so it is not suitable for sensing the fast rising edges of the switching current.

    You can use a resistor shunt sensor followed by a differential amplifier to implement current sensing in the buck circuit.

    This is what the block  a1 in the attachment above is trying to show.

    Sorry for any confusion

    Regards

    John