This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76930: bq76930 can regularly to boot up or not?

Part Number: BQ76930

I have a product design that use 2pcs BQ7693003. I can read the battery voltage and current normally when I use DC power supply to charge.However, when I use the customer's charger to charge the battery, I will encounter the situation that the battery voltage is not updated or the current is not updated.I have found out the reason. The quality of  customer's charger interferes with my work of BQ7693003. Excuse me, can I regularly go to boot up BQ7693003 or not? Or is there a better way?

Thank you very much!

  • Hi Skate,

    I am not sure I understand. If the BQ76930 is going into Ship mode, then a boot signal to the TS1 pin is needed. This can be done any number of times. However, it is important to understand why the device is going into Ship mode or why it is not able to report voltage and current. This is important to make sure something is not being damaged over time.

    Best regards,

    Matt