Hi,
My customer is looking for a step up DC/DC solutions with the following conditions:
- Vin is 5V to 20V
- Vout is 12V / 3A.
- if Vin is 12V or higher, the input can be connected to the output directly and by-pass the DC/DC.
- Small footprint.
Is there such a solution available ?
Regards,
CM.