This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA/Spice/LM3478: Adding pulse skipping feature for simulation

Part Number: LM3478
Other Parts Discussed in Thread: TINA-TI,

Tool/software: TINA-TI or Spice Models

Hi Team, 

On of my customer is looking for below details. Please help. 

For LM3478 spice model : is it possible to add pulse skipping feature at low load conditions in the spice model? This means when I do spice simulation with this model I should be able to see Pulse skipping at Low load conditions ( Vin max =19V at 105C).

Do you have a closed loop model for a simple flyback with LM3478 ( accurate spice model)  using TINA TI ?