Does BQ34110 has reverse battery protection. ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Batt,
Can I use diode in series with IC Gnd ( Anode to IC GND pin and cathode to system GND) to protect IC from rev voltage. If yes. does it affect device performance as IC GND level is shifted by diode drop.
Regards
Dilip
Hi Dilip,
No, that will not work. The bq34110 depends on an accurate reading between PGND and GND, A 0.7V shift would be too high.
Batt,
It is not clear from your reply which Que you answered ?
Que1) Can I use diode in series with IC Gnd ( Anode to IC GND pin and cathode to system GND) to protect IC from rev voltage.
Que2) If yes. does it affect device performance as IC GND level is shifted by diode drop.
Batt,
Adding to this thread, what is the best way to do reverse battery protection with the BQ34110?
I see adding a load switch controlled by another dedicated microcontroller as one option but wanted to see if Dilip's method of a diode or ideal diode (20mV) forward voltage drop could be used?
Appreciate your feedback,
Jason
Hi Jason,
You are better off using a switch. A drop across the diode is too high and we depend on the shift between GND and PGND to be small. So, do not use a diode.