This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23880: TPS23880 standby power comsumption

Part Number: TPS23880

Hi Experts,

What is the standby power consumption of TPS23880?

  • Hi Kane!

    The TPS23880 device alone requires a maximum of 12 mA from the VPWR supply. Together with the recommended VPWR range of 44 V to 57 V would indicate a standby power consumption of 0.528 W to 0.684 W. More information on VPWR supply sizing and recommendations can be found in section 10.2 of the TPS23880 datasheet (Power Supply Recommendations: VPWR).

    The datasheet can be downloaded from this page --> http://www.ti.com/product/TPS23880/technicaldocuments

    Thank you for reaching out to us and don't hesitate to let us know if you have any more questions!

    Aidan Davidson