1- For the BQ35100, could you give me some information on the maximum current ( ICC_ACCU Max) that the device pulls when it is running in ACCUMULATION mode (GE=High and GaugeStart() received).
2- According to the datasheet, when the BQ35100 is used in the ACCUMULATOR mode, and GE =High, ICC_ACCU=130µA and when GE =LOW, ICC_ACCU=0.05µA. I would like to know where the rest of the current goes when GE=LOW.