Part Number: LM5164
Hello,
I have a design that I extracted from Web-bench. During verification of the power supply, when I powered the board with 70V DC the IC exploded at pin 2. I have looked at the Absolute Maximum Ratings and don't see anything the design is violating. In another instance, the board was working fine at 60V; however, when I increased the load on the supply, the LM5164 also died. The load current does not exceed 0.4A in worst-case use (actually closer to 0.37A).
I would appreciate any suggestion. I'm posting a picture of the failure and the schematic (which like I said, I derived from Web Bench). Note: the circuit Vin is only supposed to reach ~98VDC in cases of failure and I designed this circuit to withstand this voltage. In normal operation Vin should be less than 30VDC.
Thanks