Part Number: TPS92640
Dear TI Team:
What is the function of the Schottky diode connected with UDIM?
Thanks!
Regards!
Eric Shen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS92640
Dear TI Team:
What is the function of the Schottky diode connected with UDIM?
Thanks!
Regards!
Eric Shen
Hello Eric,
The main function is to allow UVLO to function when PWM is high, it is a multi function pin. If there was no diode the PWM connection would not allow UVLO to function from the three UDIM resistors since PWM would take over (if it is being used).
Best Regards,
Hi Irwin:
Thanks for your reply!
My customer PWM input is 5V level , 2KHz,
1, If the PWM signal is connected to the negative (positive is connected to UDIM) of the schottky pole, how does the PWM signal input the UDIM PIN?
2, Why choose schottky diode, how to choose the schottky diode specification?
Thanks!
Hello,
1) If a 5V PWM is applied the common or return ties to the circuit common or ground. The positive going PWM ties to the PWM (cathode of the diode). When PWM is low the diode conducts pulling UDIM below 1.276 minus the hysteresis of UDIM turning off the TPS92640. When PWM is high UDIM is pulled high by the UDIM resistors (diode is, most likely, reverse biased and not conducting).
2) The diode is not that critical for 2 KHz PWM. They can use a BAT56, BAS40, or even a 1N4148 (not a Schotty diode) or anything similar. It just has to be able to pull UDIM below the UVLO threshold, including the hysteresis.
Best Regards,