I'm using a LM27761 to convert 3.3V to -1.5V, a picture of my schematic is shown below
I think my deviations from the layout guidelines have corrupted my VCPOUT line, as i'm getting ~-1.098V on the CPOUT pin and thus no output on VOUT. I've included a screenshot of my PCB layout and was wondering if it is possible that a parasitic inductance could have caused this corruption, or if the issue could stem from something else, like a contact issue (the package was hand-soldered) or perhaps something wrong with my schematic design. All the caps are ceramic and rated for at least 10V, resistors have 1% accuracy and rated for 0.1W.
U6- LM27761
R8- R1 (11.8k)
R9- R2 (51.1k)
C12 - CIN (4.7 uF)
C19 - C1 (1 uF)
C20 - CCPOUT (4.7 uF)
C14 - COUT (2.2 uF)