Other Parts Discussed in Thread: TPS54427
TPS562200 12.0V Input gets disrupted for 100us due to a new type of expandable subsystem powering up. During this time the TPS562200 3.3V falls linearly to 1.875V over 300us, holds flat for another 300us, and then ramps linearly back to regulation over about 500us.
The 3.3V load is about 500mA and is not appreciably changing during this disturbance.
This circuit has been in production for 2 yeas without issues and this is a newly identified incompatibility. Similar systems that employ the TPS54427 are riding through the same disturbance without issues.
Suggestions to diagnose and cure are appreciated.