Part fails when plugging into a power supply. The power supply is set to +24V. The part does not fail when I turn the power supply on and off. The part fails when I plug the the positive lead into the power supply. When turning the power supply on and off there is no overshoot of the Vin voltage. But when plugging the positive lead into the turned on power supply the Vin voltage will sometimes go beyond +50v. I can sometimes see a small spark at the positive lead as I plug in. Looks like this overshoot is failing the part. I need to clamp the Vin to less than +42V. Any suggestion?