This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC29950: Is it possible to enter dc?

Part Number: UCC29950


Hello team,

We are designing 150w power using ucc29950.

If input is ac (90V~264V), there is no problem. If input is supplied by dc (130V~375V),

the operation is caused by ac1,ac2 pin problem. I don't think I can.

There is a way to operate ucc29950 ic with input dc.

If there is a way, how do you configure ac1,ac2,sufs pin?

Thank you in advance for your support