Other Parts Discussed in Thread: TPS53317
Because over current limit only show typical value in TPS53317A and TPS53317 datasheet .
Can you help share how many max and min value for TPS53317 adn TPS53317A ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Positive OC 7.6A: min=6.8A, max=8.7A
Negative OC: min=6.6A, max=10.2A
I don't find data for positive OC 5.4A. The estimated min is 4.2A and max is 6.5A.
Thanks
Qian