Other Parts Discussed in Thread: BQ25895M, BQ25606
Hi,
The Default Battery Charge Voltage of BQ25890 is 4.2V.
Question1: How to charge a 4.35V battery? Just change the VREG (Charge Voltage Limit) in REG06 to 4.35V? Is that enough?
Question2: But, since the VREG must be written with I2C and in my system, the CPU may be powered down when charging. In this situation, the charge voltage would be the default 4.2V. The battery cannot be fully charged. Will that damage the battery if the charge voltate is 4.2V not 4.35V, for a 4.35V battery? Or will that shorten the life of the battery?
Question3: Is there any way to make the 4.35V charge voltage without software programing? Or, is there any other Power Maganement Chip in TI, with a default charge voltage of 4.35V?
Thank you.