We designed DC_DC converter using UCC28950.
Vin:200-240VDC, Vout: 22 to 26VDC, 17A output. Working fine.
But, At Vin 200VDC and at Vout 26VDC, when output no load it gives 26VDC. fine
but, the moment when i put 2A load, output voltage drops to 23.5V and output slowly increases to 26V after 3 minutes.
I adjust error amplifier / compensation circuit , but no use.
Here i am using transformer turn ratio 7 and inductance of primary was 1.6mH, Output capacitance: 4500uH and input capacitance 1400uH
and output inductor value is 15uH.
Here i am attaching schematics also. Please suggest us to solve this problem.SCHEMATIC _ 02.CONTROLLER.pdfSCHEMATIC _ 01.POWER STAGE.pdf also