This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5023: Application design does not match application note

Part Number: LM5023


Hello,

The TI page shows a clear application note for the LM5023 in a design called PMP8677. In the LM5023 datasheet Pin 4 (comp) is connected to gnd through a cap.  In the PMP8677 design this cap, C15  seems to be replaced by a part with a value 49.9k. This suggest a resistor. Can you conform and clarify?

As well,
In the LM5023 datasheet pin 5 is connected through a 499 Ohm resistor (R17). In the PMP8677 design this value is suddenly 4.99k. Which is correct?

And to continue,
A quick evaluation of this design could really help. Can gerbers  for this board be made available?


Thanks!!