For the TPS54620 what are the conditions which would cause SS/TR to be pulled low prior to PG?
The SS/TR pin is connected to a voltage divider which remains steady during this event. The divider voltage at SS/TR is 1.5V.
Thanks,
Allen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For the TPS54620 what are the conditions which would cause SS/TR to be pulled low prior to PG?
The SS/TR pin is connected to a voltage divider which remains steady during this event. The divider voltage at SS/TR is 1.5V.
Thanks,
Allen
Hi Allen,
There are two scenarios I can think of below. Based on these thoughts it would be interesting to repeat this test while monitoring COMP and EN.
Best Regards,
Anthony