This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Recommended railway power supply scheme



Dear all :

       I have the following power scheme requirements

Input voltage:DC-160V
Output voltage:(1) DC-24V;(2) DC-48 V
Output power:100W
PCBA size:1/2 brick, 1/4 brick each provide one solution, can be the same solution

Please recommend a low-cost solution?

Thank  you!