Hi,
I'm posting this question on behalf of my customer. It appears they're having trouble with the EVM of the BQ78350-R2.
we have a problem with the parameter setting of BQ78350-r2.
After each cycle the learned full charge capacity decrease by the value we set in FCC learn down.
The design capacity is 15042 mAh. Normally the pack capacity should be about 1000 mAh above this value, but every time we discharge the pack the learned full charge capacity drop by the specified FCC learn down.
What can be done to correct this?
Thanks,
Lauren