Part Number: BQ25890
Hopefully a simple and easy to answer question but I want to be 100% clear:
If 5V is introduced onto the VSYS rail (from the charger) when the OTG is activated and producing 5V internal from the battery, what does the chip do?
-Prefer the incoming 5V?
-Block the incoming 5V?
-Shut-down the OTG?
Should I design some kind of filter for this to block the potential of incoming 5V or does the chip handle this with adequate safety?