Other Parts Discussed in Thread: LMR64010,
Hello TI;
We have some EVAL BOARDS (AN-2183 LMR62014/LMR64010 Demo Board) we have been testing with the LMR62014 to obtain a 12V output from a 3.5V to 8.5V input, so far it has worked fine, but we have some questions:
1- If our application is below 40mA can we use a different "D1" ? The idea would be to use one with less current capacity and cheaper, since we will never go farther than 50mA.
If this the case, does TI have some PN that could work for this?
2- If our application is below 40mA can we use a different "L1" ? The idea would be to use the smallest and cheapest inductor without sacrificing the performance.
3- The LMR62014 and the LMR64010 seems to be pretty similar.
3a - Why if the LMR64010 has lower power capacity is more expensive? Are there any performance difference or any other difference besides the Current?
3b- What is the lifecycle of these 2 devices any plans of any of these going EOL?
3c- Do you recommend anyone specially? If this is the case, why.
Please answer all questions.
Regards;
Luis
Regards;
Luis