Other Parts Discussed in Thread: BQ24210,
I will be using a relatively small solar cell to charge a Li-Ion battery. My application is tolerant of slow charging.
Solar panel: 5V (6VOC), 30mA-34mA
Battery: 18650 3.7V 2200mAh, no thermistor
This is a simple application with no need for monitoring functions. Just basic charge management and battery protection.
I've been looking at the BQ24210 solar charger and BQ25505 boost charger. The 24210 is easier and less expensive to implement.
Does anyone have a recommendation for which part to use, or another part that would be better?